Hello teams,
Previously, I created a thread with
" I have been testing TPS65917 EVM.
I powered the TPS65917EVM with 3.8V and 1~3A.
I have tested the PMIC several times and all of a sudden, I see that the power isn't going in enough.
When I set the voltage as 3.8V, range and limit of current as 3A, the voltage only goes in 1V while current goes in 3A."
As long as I checked, this EVM is damaged.
I purchased this EVM from Digi-key and would like to know if there is anyway that I can get EVM repaired or replaced?
Thank you.
Sincerely