Hi,
I am using LM5017 DC-DC converter IC.
Maximum Input voltage can be 92V. (Currently we have checked upto 32V)
OUtput current required = 300mA.
Inductor used - 470uH and 220uH.
Our observation - The output voltage is fluctuating with error of 100mV. The FB voltage as per datasheet should not be greater than 1.25V, but we observed voltage of 1.3V
How can we make our output voltage constant?