Hi Support team
My customer is working on a design with the TPS650231RSB. He wants to use two of the DC/DC in an adjustable mode. Will send schematic via email once assigned.
He is trying to do an error analysis over temp and needs accuracy tolerance on the internal reference. Can you supply this?
Customer comments
Regulator DCDC2 is being set via resistor divider to supply 3.3VDC.
- See below embedded schematic snippet.
- Output Voltage= (1+680/150)*(0.6V)= 3.32VDC
- Where in the spec is the min and max values of the 0.6V internal reference?
- At room temp and over temperature.
- I want to calculate the min and max regulator output voltage.
- Thank you!
Regards,
Jeff Coletti