Other Parts Discussed in Thread: PMP10200
Hi Team,
I need a controller recommendation for a full-bridge isolated boost topology, similar to what is shown below.
The current specs I have are the following...
- Input voltage is varied by a mechanical component and can range from 33V to 400V. These are line-to-line voltages.
- Output voltage should be 28-33V with some flexability
- Output current will be 2-3A
I've proposed a flyback topology using the UCC28700 (such as PMP10200) but due to the wide Vin range and a desire for a linear control-to-out function the customer has requested a full-bridge boost proposal.
Thanks for the support,
Hayden