In PMP8740 If I dont want parallel connection of power supply feature then what changes I should do? my email id is engg5@adordigatron.com
Anjana
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In PMP8740 If I dont want parallel connection of power supply feature then what changes I should do? my email id is engg5@adordigatron.com
Anjana
Hello Anjana,,
If you don't need any parallel function, just do not use (do not populate) U14 (and passives), Q36, Q37, Q38, Q39, Q200 (and other components associated), remove the CAN-Bus connectors and remove U5, Q5 and passives.
On the display and push buttons, just set the power supply as "stand alone".
Best regards,
Roberto
But i want CAN communication. my requirement is i want only dc-dc converter with all protection features and CAN communication
Anjana
Anjana,
If you don't need parallel functions but want to keep CAN communication, just remove U5, Q5, D22, D5 and related passives, and set the power supply as "stand alone". This way you will have available on the CAN bus all information about output power, voltage, current, status etc.
If you don't even want precise current limit (needed by a battery charger), but your application is just a power supply, you can remove the current sensing resistor R92, U11 and passives, U1B, Q4, D3 and passives associated to U1B. This way your system will limit the output current according to the current sense transformer T1 and current sense resistor R34.
Thanks,
Roberto