Hello, I have a few questions regarding the BQ24076 Battery Charger.
1) What voltage battery can I use with this chip. The datasheet says V_bat is 4.4V, but I'm not sure if V_bat is the constraint on the battery voltage or the voltage at which the IC charges the battery.
2) Can I use a 3V CR2032 coin cell battery or does it have to be a certain voltage?
3) Does the IC take care of full-charged and low-charged voltage since the CR2032 battery can range from 2.3-3.3V?
4) What is the output voltage? The datasheet has two ranges: Vout = V_bat and 3.41V. I'm not sure which is the actual output.