This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL4242: Please explain the block diagram.

Part Number: TL4242

Hi team

TL4242-Q1 is in use.

I do not understand the block diagram in the datasheet.

Is it possible to describe as much as possible?

Thanks,

TM

  • Hi Taemin,

    What is the specific question that you have on this diagram? It's not easy to explain the whole diagram without a specific aspect. Besides that, a block diagram is just a simplified diagram of the device. The detailed feature description and typical application of the device is included in the datasheet. You can follow these description for the design. Thanks.

    Best regards,
    Shirley He
  • Hi Shirley He

    Thank you for your reply.

    If the overall description is not easy, can you explain the Bias Supply, Bandgap Reference, and Comparator sections?

    I ask politely.

    Thanks,

    TM

  • Hi  Teamin,

    The bias and bandgap voltage reference is used to produce a temperature independent voltage reference which is widely used in integrated circuits. The comparator is used to regulate the reference voltage at REF pin at 177mV(typically).

    Best regards,

    Shirley He