Other Parts Discussed in Thread: BQ50002A, BQ500511, BQ50002, BQ25100, BQ51003
Hi,
I am struggling to find the difference between the bq500511/bq50002 and the bq500511A/bq50002A combination.
The only thing I seem to find in the datasheet of the bq500511(A) is that the bq500511A has "Improved Demodulation Algorithms Provide Robust Communication in Noisy Environments". For the bq50002(A) I found this sentence missing from the bq50002 version: "When paired with the bq500511A the offset in the bq50002A current sense amplifier is dynamically compensated, which allows accurate FOD performance".
Am I correct in assuming the A version of the combo is more robust and will have better performance, or is this only situational?
The main reason why I am asking this question is because we have an issue with our TX charger based on the reference designs with the non-A combination. With all casing and realistic spacing between the coils, charging seems to start but after 20-40 seconds, LED_B either starts blinking slowly (LED option 1, so DPL I am assuming) or is constant on (what is the best way to debug source of fault?). When we remove some material and hence decrease the distance between the coils, the charger seems to work fine (LED_A remains blinking). It seems that we are operating at the edge for the current configuration. I was wondering if using the A combination, we would move more towards the safe end of the edge.
Thanks!
Wout