This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40170: PMP6680 solution about FET selection

Part Number: TPS40170

Our customer would like to design the following power condition circuit.

Vin: 40V
Vout: 12V
Iout: 20A

I checked PMP6680 design because input and output condition is almost the same.
However TI's FET is not used in this design.

Do you have any reason why you didn't use your FET? Is it thermal concern?

If it is possible, we want to use parallel CSD18537 and CSD18563. Do you have any concern about this?

Best Regards,
Kohei Sasaki