Other Parts Discussed in Thread: LM4041-N
1 I plan to go up the clipping voltage 3.5V to 5V of BQ25071-Q1
I'm going to insert 1.5 V zener diode between Out pin and BAT pin. Does this work?
2 According to the Block Dia. in the Datasheet, ISET pin voltage is compared with 1.5 V.
Therefore, charge current may be 1.5 A as register R1 (ISET-GND) equal to 1k ohm
Am I wrong?