This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563209: design for low current application

Part Number: TPS563209
Other Parts Discussed in Thread: TPS561208, TPS560200

I need to use this part for low current output. Input is 12V and output is 3.3V@0.2A for one application and for another application input is 12V and output is 5V@0.15A. It is my understanding to use higher inductor around 10uH instead of 2.2uH as recommended in the data sheet. In data sheet table is provided for selection of inductor, output cap and feedback resistors but not provided what is the input, output current. Especially inductor value can not be generalised as it depends on input  and  output current. In webench also it is suggested for 2.2uH, and 3.3uH for these applications. Is there any specific reason to use these inductor values? Please suggest. Also please suggest for the procedure to reduce over current limit. 

Thanks, Harikant