Hi Team
TPS1H100-Q1 has Abs Max CL Voltage = 7V and Abs Max CL Current 30mA.
my question is IC has internal clamp voltage for CL pin ?
and how about our other hide side drivers also have internal clamp for CL pin ?
CL pin's internal Vclth is 1.233V for curren tlimit, so that normally CL pin will not go above 1.233V.
however, I would like to know the worst case.
for example(just example...),
with Rcl = 1Kohm, assuming 10mA flowing out from CL pin by Iout/2000 = 20A/2000,
it will make 10V(= 1Kohm x 10mA) on CL pin which is above Abs Max 7V.