This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90120: Clarification regarding UCD90120 implementation and usage

Part Number: UCD90120
Other Parts Discussed in Thread: UCD90SEQ64EVM-650, ,

The Datasheet layout guidelines recommend V33A (pin 46) to be connected to V33D through a 4.99 ohm resistor.

Q: V33A on the UCD90SEQ64EVM-650 development board is connected to V33D through a 220 Ω ferrite bead, differing from the above. What should the correct implementation be, or what are the compromises of one approach over the other? 

PMBus Address Bins (Table 8) are defined depending on a resistor value connected to an address pin.

Q: To confirm my understanding of the above, is Address Bin 5 defined by connecting a resistor value between 41.2 kΩ and 53.6 kΩ or  31.6 kΩ and 41.2 kΩ ?