I'm using PTN78000H to convert 28VDC to 20VDC. In order to protect several MOSFETs that are between the 28 and 20 VDC rails, I plan to place a 15VDC Zener diode between the input and output of PTN78000H. This will pull up the output of PTN78000H when 28VDC is applied to the input. Will pulling up the output of PTN78000H damage the converter?