Other Parts Discussed in Thread: LMZ14202, , LM3880, LMZ14203
Hello
I have a concern I try to command a LMZ14201 and LMZ14202 , following the proposed schematic with the resistor divider
( LM3880 is set with 100 K resistor ballast and works fine without LMZ connection )
LMZ14201 Vin is 12V
test result
1) straight drive EN with a 5 V DC source that work
2) straight drive EN by using the LM3880 I destroy the LM3880 after several ON/OFF Cycles
3) resistor divider ( 9.1K / 20K ) EN by using LM3880 = I do not succeed to drive the LMZ14201 I measure 1.2 V out of the LM3880 after the ballast
Does someone can explain where is the problem ?
Does someone now what is the current level at the EN PIN LMZ14201 / 202 ?
Thanks
David