This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF3312: REF3312 Turn-On Settling Time (to 0.1%)

Part Number: REF3312


Hello,

 

My customer is looking for 1.25V reference having <500us Turn-On Settling Time (to 0.1%) and considering MAX6023EBT12 because it’s Turn-On Settling Time (to 0.1%) is very fast, 30us.

 

The REF3312 datasheet says Turn-On Settling Time (to 0.1%) is 2ms at CL=10uF. And minimum capacitive load is 0.1uF. Can you say when CL=0.1uF, the Turn-On Settling Time (to 0.1%) would be 20us (2ms/100)?

 

Best regards,

 

K.Hirano