Other Parts Discussed in Thread: CSD16321Q5, CSD17556Q5B, CSD16322Q5, CSD16327Q3, CSD, CSD17301Q5A, CSD17303Q5, CSD17308Q3
Hi,
I am working on development of an application, which requires switching load through a mosfet. The configuration will be as High side switch. The applied voltage will be under 7V and the current drawn will go to more than 7A .but most of the time it will be under 5A. The mosfet needs to be controlled by a 3.3V logic MCU. i would like to directly drive the mosfet from it, without any gate driver, ie, GPIO driving the gate. The operating frequency will be 1kHz, but this is yet to be decided. But 10kHz will be the ceiling. Other requirements are low Rdson, low switching losses (should not get heated up).
I am looking at CSD 16325Q5 for it, though i have other options like CSD16321Q5, CSD17303Q5 and CSD17301Q5A. I have samples for these. Other options, which appear useful are CSD16322Q5, CSD17556Q5B and CSD16327Q3.
Are the above mentioned FETs suitable for my application? Or any other ones would work better?
Thanks