hello team,
I am looking for a buck regulator,which has such features:
input 5V output 4.6V,max input voltage can exceed 12V
low high-side and low-side MOSFET on-resistance
output current can exceed 4A
low cost is better
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.