I want to use a TPS71701 as a voltage regulator with a DAC output range of 0-3.3V. The DAC may not output 0 but it does not affect use. The regulator output range is 2.5-5V.
Which is the VREF. By the way, if the TPS71701 chip is suitable, the fluctuation of the adjustment is much.
Parameter |
Value |
VREF |
|
VNOM |
3.75V |
ΔVDAC |
3.3V |
ΔVMARG |
2.5V |
R2 |
324kΩ |
VDACN |
1.65V |