This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ14201: I need a example circuit to drive safely EN from logic in 5 V DC

Part Number: LMZ14201


Hello

After one day without access to the forum due to server problem

I need if possible a example of circuit able to drive the EN pin of a LMZ14201 from a  logic level 0V / 5V DC

the floating level of the EN PIN is 6.5V when floating so I burn my logic component 5V

I am clearly lost and deeply lost as the doc say that logic level is 1.18 V so I do not to burn the LMZ14201  with 5 V

Thanks for your help

David