Other Parts Discussed in Thread: SN74AVC16244
Hi,
I need to cascade 90 TLC5928 !
I have designed a board with 9 TLC5928s in cascade and I need to cascade 10 boards.
Each board is 20 cm long, the result is a 2m long line. It's a 190x8 pixels LED display.
I have added a CD4050 buffer to each board (output signal) for better signal quality.
When I send data to the line, the first board is OK, but the 2nd board as 1 bit lost and the 3rd as 2 bit lost, etc.
When I search in the datasheet, I have found that in page 7: SIN is read on rising CLK and SOUT change on rising clock too.
With oscilloscope I have observed that the CD4050 add a small delay on CLK, and that is suffisant to break the signal.
I have added a 1.5nf on the last SOUT that make the rising too slow and they are no bit lost with this "workaround".
Is exist a CD4050'equivalent with best speed ?
Regards,