This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25085: LM25085 100% Duty cycle

Part Number: LM25085

Hi Sir,

we are look for LM25085 100% Duty cycle solution for  12V~26V to 12V/5A application.

But the TI WEBENCH show the "Calculated duty cycle exceeds limit".

is LM25085 right solution for this application? or any suggest Synchronous Buck?

Hugo

  • HI,

    This could be because there is Rds on of the MOSFET that Webench taken into calculation.
    You might want to increase it to 12.5V or so for the sim to run.

    As far as datasheet, it is capable of running 100% duty cycle as one of the feature.

    Thanks
    -Arief