This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24038: USB Input voltage Max (9V) ?

Part Number: BQ24038
Other Parts Discussed in Thread: TPD1S514

Team

Is there any damage of BQ24038 if customer input over 9V to USB input ?

According to the Datasheet, BQ24038 just use 7V USB input.

If there is problem, i think customer should use Over Voltage Protection.

If so, could you also recommend the OVP chip ?