This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61195: Dimming mode

Part Number: TPS61195

Hello,

Our customer use the TPS61195, have two questions.

Q1) The customer using the dimming mode under  the following conditions.

PWM interface

Frequency of the dimming : 20kHz

minimum duty : 10%

Which mode should the customer select?

Q2) The pin function of the EN pin

It is mentioned "SDAble and Disable Pin" at the PIN FUNCTION table on the datasheet.

What it means "SDAble" ?

Best Regards,

Naoki Aoyama