Other Parts Discussed in Thread: TDC1011
Hi,
i want to use the TDC1011 to measure water depths and not the PGA460 because of its 11m distance limit.
Is there a circuit/IC from TI that can drive 1kW transducer from a LiOn battery?
The DR8870 IC can supply 3.6A output current with 45V as input power. This makes an ouput power at 157.5W right?
So far i have a custom board with TDC1011 sending burst to UCC27531 and it drivers the transducer with a 28V from a step up converter TLV61046A.
Since the TLV61046A has a current limit of 980mA and UCC27531 output the burst with 28V amplitude, the output power on the transducer can be maximum 27,44W right?
So i have to increase 35 times more the output power to get 1kW, but how can i do this?