This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMR14010A: LMR14010A buck converter with 3.3 V output

Part Number: LMR14010A
Other Parts Discussed in Thread: LMR14030, LMR14020, LMR14006, LMR16006

Tool/software: WEBENCH® Design Tools

Hi,

I would like to use a LMR14010A buck switcher as converter from 10 V - 17 V to 3.3V, with max. current output of 0.3 A. If I put this values in WEBENCH® Designer I get an error: Design is unstable. Why I get this error exactly?

Many thanks,
Dejan.