This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: LM5116

Part Number: LM5116

I am developing a DC DC controller with input voltage ranges from 13V to 90V with output voltage of 12V. I have configured the board for about 3A load current. (LM5116MHX/NOPB)

I developed around 5 boards for testing. My observations were as follows:

Board gave only 3.9V output What might be the fault in these boards? is there any other parameters that i should verify? I have almost implemented the same circuit as that of LM5116 evaluation board

We used MOSFET FDMS86200 and BSC350N20NSFD and Bourns PM2120-560K-RC

Regards

H.J.Hamsaraj