This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM53603: LM53603 - Q1 input voltage range.

Part Number: LM53603

Tool/software: WEBENCH® Design Tools

I want to use LM53603 as a buck converter to step down 5V DC to 3.3V DC. i have noticed in datasheet's application note that everywhere they have mentioned input voltage range as 6V to 36V but input voltage range says 3.7 to 36V.

Even in efficiency plots, minimum input voltage is shown as 7V.

can any one please confirm that LM53603 regulator does work at 5V DC.

regards,
abhiraj