Other Parts Discussed in Thread: OMAP-L138, TPS3805H33
Hi Berner,
Good day!
After a long exploration, I realized that the PMIC-TPS65070 is a better option for my application. I have few Queries on TPS65070 PMIC Hardware design, could you please clarify these:
1. Is it okay to keep TS pad UNCONNECTED if I do not use TS pin on TPS65070?
2. Are the ENDCDC1, ENDCDC2 pins controlled by Digital logic of High(3.3V) and Low(0V) by a micro-controller on my board?
3. Is it okay to keep DCDC3 related pads(L3, VDCDC3. DEFDCDC3, ENDCDC3) UNCONNECTED if I do not use DCDC3 output on TPS65070?
4. wLED, and Touchscreen interfaces are not being used, Is it okay to keep them UNCONNECTED?
5. Is it possible to control(ON & OFF) LDOs 1&2 through I2C interface as their Enable pins are not given out??
In the datasheet, it is not mentioned about unused pins.
Thanks in advance.