This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92210: Is TPS92210 suitable for 150Vout@700mA application?

Part Number: TPS92210
Other Parts Discussed in Thread: PMP5652

Hi Support team,

My customer found a reference design PMP5652 using TPS92210, but their output current needs to be doubled of PMP5652. Is TPS92210 still applicable for their design? Here is the spec requirements:

- Input voltage: 200-440Vac

- Output voltage: 100-150Vdc

- Ouptut current: 500mA to 700mA

- Efficiency requirment: 90% @ 230Vac (at full load)

- PF requirement:  0.98 @ 230Vac, 0.93 @ 480Vac,

- THD: THD<20% with load ≧ 50% at 230/347Vac input

- Dimming: 0~10V analog dimming

Or please suggest better solution for the listed spec.

Thank you.

Best Regards,

Wei-Hao