Other Parts Discussed in Thread: CSD18510KTT, LM5170, CSD19535KTT
Hello all,
I have 3 LM5170's in 6 phases operation in boost mode operation to step up voltage from 24V to 28V and current capability of 100A. The problem is, when I start converter for the first time, everything works fine. When I shut down the source and turn it on again in few seconds the converter is shorted to ground through Low Side transitors (it is doing the same if it is not loaded or loaded and I know it because they always burn). I thought that is caused by Crrs parasitic capacity of transitor but I was wrong and choosing transistors with lower Crrs did not helped( I have used CSD18510KTT and changed to CSD19535KTT) . When I let converter stand disconected from source for a half a of minute the converter starts successfully. I cant figure what can cause this problem. Maybe it can be caused by current loop but I tried to change values of those capacitors and resistor, but nothing helped. If I can measure something or need values of some parts which, could helped please let me know.
Thank you in advance.
Kind Regards,
Erik