This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16006: Switching with light load

Guru 16770 points
Part Number: LMR16006

Hi

I want to confirm LMR16006 operation under following condition.

Vin:12.5V

Vout:12V

Iout:50mA

I obtained following waveform using LMR16006XEVM.

1. CH1:SW, CH2:VOUT

12Vout seems to be regulated. 

Is the switching wave correct?

2.

The following is obtained when VIN is decreased by 12.3V.

Vin is 12.3V but the output 12V is regulated.

Could it be possible to regard that the  SW waveform in upper figure is correct ?

BestRegards