hi, I'm a FAE of TI, My customer has a question about LM5110
from the Datasheet, we can know that the maximum input voltage level of LM5110's IN_A and IN_B pin is "IN to IN_REF -0.3-15V"
so we just need to consider the voltage between IN and IN-REF? Don't need to think the voltage between IN and VCC?
For example:
if we connect IN_REF and VEE, and IN is 12V, VCC is 9V, so the device also can work normally?