We are using the TPS3306-18 with Vdd = 3.3V and Sense1 = 5V, Sense2 = 1.8V. At ~20C power up we are seeing the part apparently latch up with the part driving reset and the oscillator not running. We can tell this by putting a FET probe on the power pins (we can see the oscillator when it runs. The Sense1 input comes up before the Vdd.
Q: is there any input condition that can cause this latch up? Transients?
We are in the process of monitoring the input pins at power up to see if any transients are occuring.
thanks for any help.