Other Parts Discussed in Thread: DCPA10505
HI sir:
When i use the DCP010505B for a 60ma load. i find that when I start up .i will be have a big current. And about 5s later it will be normal. I use it refrence the datasheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI sir:
When i use the DCP010505B for a 60ma load. i find that when I start up .i will be have a big current. And about 5s later it will be normal. I use it refrence the datasheet.
Lei:
Request your complete schematic for the DCP010505BP including Vin input and output capacitors type and capacitance value. location of input capacitors.
1A.Is the DCP010505 Sync. On/off pin, pin14 used to control the on-off function is it open/ no connection>
2. t what is the 5V input power source DCP010505BP, current rating and inrush current rating?
2a. When the initial input power is applied does the output voltage t is possible the DCP010505 input inrush current is loading down its input 5V power source.
2b. Place Scope probe on the DCP010505BP input power source What is the DCP010505BP Vin 5V input data characteristics during power up mode?
2c. Is the 5Vin voltage dropping below 4V during initial power up.
Tom
Hi Lei:
anks for the schematic of the DCP010505,
Based upon your data comment It appears there are (2) DCP01050 on the 5V input power source(M1171-5V) including LM1171-3V3
Based upon your data comment , It appears there are (2) DCP01050 on the 5V input power source(LM1171-5V) including LM1171-3V3out voltage .
A,. DCP010505 series required minimum input ceramic capacitance is 2.2µF . 2.2µF ceramic capacitor is be located very close to and between input Pin1 ( Vin(+) and pin 2( Vin(-)
Input inrush current during startup period can over load input 5V power LM1171-5V) drooping the input voltage to below 4V.
See below for spec.DCP010505 details on inrush current
2. There is another direct replacement converter , 1W, DCPA10505P available with reduced soft start-up in-rush current. Same package type and same pins functionality It is a direct drop in replacement for the DCP010505BP.
Tom