This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53314: A questions about the current limit for TPS53314

Part Number: TPS53314

Hi ,

 Our customer wants to confirm if below OCP setting is okay or not, since no maximum current range and tolerance on datasheet.

 Can you help to check and give a comments for below application?  Thanks.

-------

The Below is for 1.8V Power Rail with TPS53314. Could you check if the OCP setting is OK or not?

Vin=12V

Vo=1.8V

Io.max=5.177A

OCP=6.7A