Other Parts Discussed in Thread: LM36010, LM3644
Hi Sir,
Now I have a project wnat to use VCSEL LED(see the spec below), input 5V, and control it on for 3ms, off-60ms, on-3ms, off-60ms......
1. can I use two LM36011 to drive the LED?
2. If I input 5V, and the Vf=2V, where is the other 3V?
3. How to control flash LED on-off-on-off...? Use STROBE in IR Mode? Is ther any timing limitation? (I want to control it as 3ms, off-60ms, on-3ms, off-60ms......)
4. Or is there any other better solution?
PS. The drivering current could up to 3A, it's kind of Laser LED. Based on driver solution, maybe the current spec could modify, but 1.5A at least.