This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596: How fast can you switch input pin 5 (ON / OFF)?

Part Number: LM2596

I designed a device that is powered by LM2596S-ADJ/NOPB. The input has a voltage from 5.2V to 8.4V and on the output we have a voltage range from 2.5V to 5.5V. I need the output voltage to be switched on at 100Hz and 50% fill. Can I connect TTL signal to input 5 (ON / OFF) with such frequency and will not damage the circuit? What is the maximum switching frequency of input 5 (ON / OFF)?