Hi I am using TPS62175 buck Regulator.
My input is 15V and Output is 3.3V , Sch is same as shown on page 1 of datasheet (http://www.ti.com/lit/ds/symlink/tps62175.pdf
Inductor is 10uH with 1A rating.
Test 1 :- Output Short ,
Method:- 50mA load was connected, Turn on the unit , 3.3V buit here then i shorted the output for 30-40Sec and remove the short , after removal of short condition 3.3V recover.
Test 2:- Power Up ( Issue observed)
Method:- 250mA load was connected, turn on the unit, but 3.3V never built up. tried multiple times. Then i reduced the load to 200mA then power up this time 3.3V built up and i can changed the load to 500mA , no problem. Question is why with 250mA load output 3.3V never build up during power on.
DC electronic load used for Testing.