Other Parts Discussed in Thread: BQ24192
Hello, in application of BQ27531 + BQ24192, NTC pin of battery is connectted to temperature detect pin of BQ27531.
BQ27531 demand negative temperature coefficient (NTC) thermistor with R25 = 10.0 kΩ ±1%, B25/85 = 3435 kΩ ± 1%.
Is there any method to change the B value setting of BQ27531 application if a 103AT NTC with different B value is used ?
Or the temperature coefficient of NTC must not be different from recommended in the BQ27531 datasheet ?