This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPS65094: Controller Datasheet Current Limit

Part Number: TPS65094

What is the current limit on the controllers?

  • The controller output current is not limited to the values specified in the Features page of the datasheet (i.e. 7 A for BUCK6 VDDQ). These current values are consistent with expectations for the specific Intel platform and were used to provide accurate characterization information in the Specifications section, however due to the nature of the controller, much higher current can be supported by modifying the FETs, inductors, output capacitors, and ILIM resistor.