Other Parts Discussed in Thread: CDCI6214,
Hi,
Our team recently created a board where we need to supply power to a CDCI6214, and this device requires a voltage supply ramp time faster than 3 ms. We have chosen to use the TPS7A54-Q1 to provide 1.8V to the device, but used a 100 nF cap on the NR/SS pin. This created a voltage supply ramp of around 10-12 ms, which has created issues for us due to the CDCI6214 power supply ramp time requirement. Please find the TPS7A54-Q1 schematic and layout below.
Schematic:
Layout:
Before reworking the board, I was able to see that the NR/SS pin voltage was a stable 0.78V, and VOUT = 1.778V, as expected.
However, after I changed this cap to 10 nF per datasheet recommendations, the NR/SS pin voltage became 0.2-0.3V, and over time, the NR/SS voltage slow reduces, almost like it is discharging somehow. The Power Good voltage is 0.2V and VOUT < 1 V.
Next, I removed the cap completely from the NR/SS pin. When I did this,the NR/SS pin voltage started off at 1.2V, and over time, the NR/SS voltage slow reduces as well. However, this time, the Power Good voltage and VOUT appear to track linearly with a voltage approximately equal to VIN.
I am not sure if this is an indication of a damaged IC or if this is expected behavior when changing the cap value. Any advice about what is going on?
Thanks,
Michael