Hi, all. I saw in the document "Powering the AM335x With the TPS650250" that we use RC circuit to do the Power-Off Sequence for the TPS650250. We can see that the sequence will DCDC1 to DCDC3 to DCDC2. When SYS_EN=0, assume that Vf of diodes is 0.7V, larger than VIL=0.4 rated in the datasheet, will it be a risk for the customer to power off the Vo_1.1? Another question is that if EN=0, the voltage of EN3.3 will also larger than 0.4V. How can we make this power-off sequence right?