This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TPS65912: PWRHOLD Impedance

Part Number: TPS65912


For the TPS65912x, is the PWRHOLD pin high impedance and, as a result, will it always need to be driven?

  • The PWRHOLD pin is a high impedance logic input. We recommend pulling this pin high to a voltage between 1.1V and VCC or low between 0V and 0.4V. Technically, it does need to be driven high or low, but only with a sub-micro Amp range current.