Other Parts Discussed in Thread: LP8555, , TCA9543A
Hi Folks,
I have an application where I need to control 40 red and 40 blue LEDs. I looked at the LP8555 chip which would allow me to control all 80 LEDs with a single chip but it's only available in a BSA package. Prototyping a BSA package isn't for the faint of heart so I avoid them if possible.
The TPS61177A looks like it will work for the input voltage range I have (2.5V - 4V from a single Li-ion cell) but they have the same I2C address. Is there a recommended method to use two or more of the chips in a design? Would the TCA9543A I2C multiplexer work?
Thanks in advance,
Richard