his schematic was verified by forum. But the physical board design has some issue . Its making the humming sound from the charge IC
Few this thing we absorbed while testing.
- when the sound absorbed above 4.67 above, and above 5.18V the humming stops.
- Input Voltage @ Vin pin of bq24090 will 4.8 and 4.67 as the input voltage vary from 4.9 to 8.8
- with input voltage 4.67,4.8 and 4.90 output voltage is not reaching up-to 4.2.
Th following are few design change in with schematic
- RISET IS 1K Draw 0.55A
- Instead of Nchannel MOSFET I M USING P channel Mosfet with BJT to gate control from the controller.
Please refer the attachment below for the schematic.
Please help me understand the issue, and help me solve it. Please revert us as soon as soon possible we have on the priority. Please revert for further quires.