Dear team,
I measured PSRR of TPS7A87 based on TPS7A87EVM these days, and I found that the result is close to the value of datasheet in 10Hz-100KHz, but the peak value is 20dB in 1MHz-10MHz, which is much lower than that of datasheet.
I read some LDO PSRR documents, and I think that output capacitor may decrease the PSRR in high frequencies. The ceramic output capacitor on EVM is 10uF (0603). I want to know why my measurements are much lower than the datasheet in high frequencies?
Attachment
1. TPS7A87 datasheet
2. TPS7A87EVM User's Guide
3. output cap(C4) in tps7a87evm
4. measurement result1 vout=4.2V_vin=4.3V_I=0.02A_rip=100mV
5. measurement result2 vout=4.2V_vin=4.5V_I=0.02A_rip=200mV
6. LDO PSRR document
http://www.ti.com/lit/an/slyt202/slyt202.pdf
http://www.ti.com/lit/an/slaa414a/slaa414a.pdf
7.My method of measuring PSRR