Hi Guys
Our customer want to use Buck convert as a current source. Input 7-15V; Output: 100mA current source; Vout is about 3.6V. They use it to charge a three series batteries(Ni-MH). Their battery vendors don't suggest that they use BQ charger to charge the Ni-MH battery. They need the constant current source to do this to protect battery. Maybe OVP and OCP are needed here.
So do you any suggestion about this application? Any proper Part to do it? It is better if we have converter integrated high side and low side drivers.
Any feedback are appreciated.
-Vincent