This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2456A: Redundant Power Supply

Part Number: TPS2456A
Other Parts Discussed in Thread: TPS2456, , TPS2456EVM, TPS25942A, TPS2410

Hi all

Would you mind if we ask TPS2456 and TPS2456A?

Our customer considers "Redundant Power Supply"  on TPS2456EVM's document figure4.
And then, they would like to configure it without seamless voltage drop during output changing.
So, is it possbile to configure using TPS2456 or TPS2456A?
We don't have EVM and could not find these wave form on the datasheet.

Our customer's conditions are as follows;
-Main power : 12V
-Sub power : 12V or less than 12V
-Load : 1.5A

If TPS2456 and TPS2456A can't realize the customer's construction, could you let us know recomended device?

We need your help.

Kind regards,

Hirotaka Matsumoto