Other Parts Discussed in Thread: TPS92692
Dear Sir/Ms.
I have already bought a tool tps92692evm-880 from Mouser.com. So when testing, I have a problem with PWM Dimming.
In the user manual, Analog to PWM duty cycle dimming range: 1V to 3V of Vdim, and Direct PWM dimming range: 100Hz to 1Khz, connect shunt pins 1 and 2 of J6 and pins 1 and 2 of J7 in the tool.
I relate the tool to STM32F103C8T6 kit, mesure correct Vdim, and Direct PWM. But the output voltage range not change. It's still at 54V with Boost Configuration.
My input voltage range: 6V-100Ah battery.
I want the output voltage at 34.9-37V to load, but I can't do that.
Would you please give us some advice?
Best Regards,
Lanh Tran